FAQ: Can I modulate the output of an N8762A using the analog programming port?

Yes. The N5700 and N8700 power supplies have an input connector on the rear that accepts 0 to 10 V to proportionally control the output when set to the analog control mode. Just keep in mind that limited voltage slew rate of the output will be the limitation factor on how quickly output will modulate. Refer to the User Manual at www.keysight.com/find/N5700 or www.keysight.com/find/N8700 for more details.

Applies to: N5740A, N5741A, N5742A, N5743A, N5744A, N5745A, N5746A, N5747A, N5748A, N5749A, N5750A, N5751A, N5752A, N5761A, N5762A, N5763A, N5764A, N5765A, N5766A, N5767A, N5768A, N5769A, N5770A, N5771A, N5772A

Applies to: N8731A, N8732A, N8733A, N8734A, N8735A, N8736A, N8737A, N8738A, N8739A, N8740A, N8741A, N8742A, N8754A, N8755A, N8756A, N8757A, N8758A, N8759A, N8760A, N8761A, N8762A

Select Home to return to the table of contents for more FAQs.

Visit our Power Products Forum for additional topics and discussions.

Read technical postings on our Power Blog – Watt’s Up?